Tips to speed up saved searches in StruxureWare Building Operation

Issue

Tips to speed up saved searches in StruxureWare Building Operation

Product Line

SmartStruxure Solution

Environment

StruxureWare Workstation

Cause

Searches should be optimized to improve performance.

Resolution

 

Your search is taking a large set of objects and checking against the text matching and then against the conditions. The more you can eliminate before checking text or conditions the better.
 
Whenever possible use the following methods to speed up searches
  • Use the 'In folder' field to avoid searching too large a section of the system
  • Do not Include properties or subservers when they are not needed
  • Specify the smallest subset of type you are able to. For example, if you only want Extended Trend Logs, do not use the Base Trend Log object.