The Exchange
Home
The Exchange
Community
Download Center
The Exchange Knowledgebase
> Article #17738
What is the Dimensions of the IWM24-GY Access Plate
LL#17738 created on Mar 30th, 2015, last modified on Aug 12th, 2015
Issue
Access Plate
Product Line
Pelco Cameras
Environment
IWM24-GY
Cause
Installation and Service.
Resolution
Print
Share
Review this Solution
Thank you for rating this article
(0 ratings)
Quick Links
The Exchange Knowledgebase Help
The Exchange
The Exchange Community
The Exchange Download Center
Cross Reference Tool
Contact Product Support
More Like This
Anti Vibration Mount Adapter For Pendant Mount 1.5 inch Pipe Thread IP Cameras.
IWM24-GY voltage output
Spectra options for mounting the IWM-GY, IWM24-GY to a Pole or Corner.
What product is required to mount the SD435-PG-E0 Spectra Pendant Series to a pole?
Dimensions of the IWM-GY and IWM24-GY