Issue
Setting up to Print a Report of Off Normal Points and Disabled Points in an I/NET System
Environment
I/NET site
Cause
How does one run a report on Off Normal Points and Disabled Points?
Resolution
There is a new feature in I/NET now that enables the user to run a report on Off Normal Points and Disabled Points. To set this up, the user needs to follow these simple steps:
- Start I/NET, log on and go to Edit, Host Computer, Network Functions.
- Select the Link that you need the Points to be printed; this displays all the controllers on this link.
- Click on the Nrml and Dsbl buttons, this sets up the controller to display these points.
- Select Summary, Off Normal Points, a list of points (if any are Off Normal) will be displayed.
- In this Editor there is a Print Button, Click on this, it will ask you for a printer that you normally print to.
-
Click OK and a report will be generated on your printer.
The same process should be followed for Disabled Points. - Select Summary, Off Normal Points, a list of points (if any are Disabled) will be displayed.
- In this Editor there is a Print Button, Click on this, it will ask you for a printer that you normally print to.
- Click OK and a report will be generated on your printer.