SSL Compatibility Table

Issue

Having difficulties determining which firmware/hardware version supports which feature. Some of main questions are:

- is my SE8000 compatible with my MPM's firmware

- Can I pair zigbee NYCE sensors with MPMs

Product Line

SmartStruxure Lite

Environment

SmartStruxure Lite Multi-Purpose Manager

SE8xxx Room controller
SE8000 Series
SER8300, SE8300, SE8350, SE8600
Ex. Viconics branding VT8000 Series

Cause

Firmware versions are frequently updated to introduce new features

Resolution

 

 

 

Room Controller Firmware

Zigbee-Module Application

MPM's Firmware

Comments

Lua4RC

1.0.7

N/A

2.13.4 and up

A script must be uploaded via BACnet or USB cable in order to view the "LUA" Menu.

ZigBee NYCE Sensors

1.0.6/1.0.7

051 - 0131R05 and up

2.13.4 and up

 

SE8650

 

1.2.0

051 - 0131R06 and up

 

2.17 and up  

SE8600

 

1.0.7

051 - 0131R05 and up

 

2.13.4 and up

 

SE8300/SER8300

 

1.0.7

051 - 0131R02 and up

 

2.12.4 and up

No label on ZigBee Module

1.0.6

051 - 0131R02 and up

 

2.7.2 and up

No label on ZigBee Module