What is IWM24-GY transformer part number?

DANGER

HAZARD OF ELECTRIC SHOCK.
Remove all power from all devices before removing any covers or doors of the system. Disconnect the power at the device and at the power source.

WARNING

ELECTROSTATIC DISCHARGE REQUIRED.
Discharge all static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.

NOTICE

COMPLEX PROCEDURE REQUIRED.
The resolution of this article has many complex steps that may result in unforeseen results if not performed correctly. If you are at all unfamiliar with the requirements, please contact Product Support Services for assistance.

Issue

What is IWM24-GY transformer part number?

Product Line

Pelco Transmission & Power

Environment

  • IWM24-GY

Cause

Blown out transformer on IWM24-GY.

Resolution

  • IWM24-GY step down transformer part number: XF02-0604-0001.