Disabling of the IR Illumination within the Bullet model cameras.

Issue

  • How can I disable the IR LEDs in my BU6 camera?
  • Is there a way to disable the IR lights from the BU cameras?
  • If I want the IR turned off inside my bullet model camera; how do I do that?
  • Can I turn off the illumination within the BU4, BU5, BU6 model cameras?

Product Line

Pelco Cameras

Environment

  • BU4 models
  • BU5 models
  • BU6 models

Cause

There is no understanding of the fact that the IR is integrated into the Bullet style BU4, BU5 and BU6 model cameras and is not something that can be turned off.

Resolution

There is no way to disable the IR LEDs inside the Bullet style cameras with the model numbers beginning with BU4, BU5 or BU6.