How to initialize or reinitialize the DX1000?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

DX1000 needs to be configued for the first time or reset to factory defaults.

Product Line

Pelco Video Management

Environment

  • DX1000

Cause

DX1000's software or configuration is corrupt and needs to be defaulted.

Resolution

  1. Press and hold the Function button. The Function Key List should appear. Keep holding the Function button.
  2. Press and release the 0 button, and then release the Function button. Enter the password if requested. The Setup Menu should appear.
  3. Using the front panel buttons, enter 1220.
  4. A screen appears and asks if you want to continue.
  5. Use the Search (<>) buttons to highlight Yes or No to erase the hard disk drive, and then press the Play/Pause button.