Pairing SED-WIN and SED-Dor (wireless window/door contacts) with a SE8000, SE7000, and a MPM.

Issue

Pairing SED-WIN and SED-Dor (wireless window/door contacts) with a SE8000, SE7000, and a MPM.

Product Line

SmartStruxure Lite

Environment

MPM

SE7000 series

SE8000 series

Cause

Quick reference / clarification

Resolution

The SE8000 can be paired to the wireless contacts with or without being networked to a MPM.

The SE7000 must be networked to a MPM prior to being paired to wireless contacts.

Always ensure the latest firmware is installed in the MPM.