Could STR150 be used with TAC Xenta 110-D?

Issue

Is it possible to use the TAC Xenta 110-D device with room unit STR150?

Product Line

TAC Vista

Environment

STR150
TAC Xenta 110-D

Cause

It is not possible to use STR150 together with the TAC Xenta 110-D device.

Resolution

TAC Xenta 110-D does not support STR150.