Could STR150 be used with TAC Xenta 102B?

Issue

Is it possible to use the TAC Xenta 102B device with room unit STR150?

Product Line

TAC Vista

Environment

STR150
TAC Xenta 102B

Cause

It is possible to use STR150 toghether with the TAC Xenta 102B device with system program 1.20 or higher.

Resolution

It is possible to use STR150 toghether with the TAC Xenta 102B device with system program 1.20 or higher by setting nciAppOption bit 14.