What power supply is recommended to provide POE to an EC-3001xxPOE-M?

Issue

What power supply is need for EC-3001xxPOE-M

Product Line

Pelco Cameras, Pelco Video Management, Pelco Transmission & Power

Environment

  • EC-3001CLPOE-M
  • EC-3001CRPOE-M
  • FEXTPS-48V

Cause

Power supply Installation information.

Resolution

The FEXTPS-48V will provide power to the Local and the remote and the IP Camera.

Note:

  • The FEXTPS-48V will be wire to the POE +/- terminal block on the EC-3001.
  • Refer to installation manual for Maximum Extended Distances