Vista webstation - HTTP GET method not implemented (SOAP-ENV:Client)

Issue

  • Cant login to webstation
  • Loginpage for webstation

Product Line

TAC Vista

Environment

  • Vista
  • webstation

Cause

Mostly  caused by that another process is using the same port as webstation do

Resolution

Run the command netstat -aonb | find ":80" in the command prompt to see what process PID is taking the port 80, If Vista is using another port change 80 to what port you use.

A common scenario is that it is the TAC Vista SmartStruxure interface that is taking the port, and that after a reboot, the interface starts up before the IIS.

Change the port used in the interface to something else