VideoXpert: Part numbers / Hardware / Software requirements

Issue

Customers wish to install VideoXpert software on their own equipment.

Customers wish to install VideoXpert using Pelco hardware.

Product Line

Pelco Video Management

Environment

VideoXpert Components

Cause

The integrator or customer does not have information regarding VideoXpert part numbers, hardware or software requirements.

Resolution

The part numbers, hardware and software requirements for VideoXpert can be found on the specification sheet which is located by clicking HERE.

The below part numbers are for Enterprise systems. If an Ultimate system is required substitute the E1-XXX-XX with U1-XXX-XX.

Enterprise Hardware with Software:

E1-CMG-SVR - Core and Media Gateway all-in-one hardware with software licenses.

E1-COR-SVR - Core server hardware and software license.

E1-MGW-SVR - Media Gateway server hardware and software license.

E1-OPS-WKS - OpsCenter workstation and software license.

E1-OPS-WKS6 - OpsCenter workstation with upgraded graphics card, enabling use of up to 6 monitors using Enhanced Decoders (D09U-A1-DEC).

E1-VXS-48 - VXS with 48 TB storage (32.7 TB effective storage)

E1-VXS-72 - VXS with 72 TB storage (54.5 TB effective storage)

E1-VXS-96 - VXS with 96 TB storage (76.4 TB effective storage)



Enterprise Software Parts Numbers:

E1-COR-SW - Core software license.

E1-MGW-SW - Media Gateway software license.

E1-NSM-1UP - Upgrade license enabling NSM5200 to support VideoXpert systems.

E1-DSS-1UP - DSSRV sofware license 

E1-COR-SUP - (Optional) Core software upgrade subscription; entitles users to upgrades for one year

E1-MGW-SUP - (Optional) Media Gateway software upgrade subscription; entitles users to upgrades for one year

 

Accessory Part Numbers:

VX-A3-DEC - Enhanced Decoder for extra monitor support (requires the Matrox video card and splitter cable) *Note* uses HDMI to connect to monitor.

3DX-600-3DMOUSE - 3D SpaceMouse Pro

Y-U0018-G710KBD - Logitech G710 Keyboard

A1-KBD-3D-KIT - Keyboard and 3D SpaceMouse Pro Combo

If the customer is using their own computer or has purchased an E1-OPS-WKS and wanting to turn that into a 4 or 6 monitor OpsCenter the below must be purchased together.

  • (1) PB08-1516-0001 - Matrox PCIex16 video card for extra monitor support
  • (1) CN17-8511-1001G - Splitter cable to be used with the Matrox Card
  • (2) CN17-8311-1001G - VGA terminator
     

Accessory Server

D09U-ACCSVR - VideoXpert Accessory Server