How to factory reset the IME Plus (Gen2) series cameras

Issue

An IME second generation camera needs to be factory reset.

Product Line

Pelco Cameras

Environment

  • IME129
  • IME229
  • IME329

Cause

The reset button cannot be found on the IME Plus cameras.

Resolution

Taken from the Sarix Enhanced IME Plus Manual 

Using a small tool, such as a paper clip, press and release the reset button once to reboot the camera.
Press and hold the reset button for 10 seconds to restore the camera to the factory default settings

Image of the reset button indicated below:

Using a small tool, such as a paper clip, press and release the reset button once to reboot
the camera. Press and hold the reset button for 10 seconds to restore the camera to the factory
default settings
Using a small tool, such as a paper clip, press and release the reset button once to reboot
the camera. Press and hold the reset button for 10 seconds to restore the camera to the factory
default settings
Using a small tool, such as a paper clip, press and release the reset button once to reboot
the camera. Press and hold the reset button for 10 seconds to restore the camera to the factory
default settings