Export and import between different StruxureWare Building Operation versions.

Issue

Is it supported to do an export from for example StruxureWare Building Operation version1.4 and import into version 1.6?

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation

Cause

It is always allowed to export from an earlier version and import to a later version but not the opposite way. With one exception in StruxureWare Building Operation version 1.7 exports from version 1.0, 1.1 and 1.2 will not be supported. The workaround if having a export file this old is to import it in version 1.6 and then export from there to 1.7.

Resolution

It is allowed to export from an earlier version and import to a later version but not the opposite way