According to the datasheet, SHD100/STP300 is IP65 rated. Any option for IP66 enclosure?

Issue

According to the datasheets, the SHD100 and STP300 is rated IP65. Is there any option for IP66 Enclosures?

Product Line

Field Devices

Environment

IP Enclosure

Cause

The datasheet says IP65, that is what we have to day.

Resolution

As today, we do not have any Enclosure for IP66 for any of our sensors.