Netcontroller 2 Comm port pinout options

Issue

Customer wants to connect MODbus meter to Comm port 4 on a Netcontroller 2 but needs to know which pins to use

Product Line

Andover Continuum

Environment

Continuum

Netcontroller 2

NC2

Cause

Customer wants to know Netcontroller 2 pinouts

Resolution

The Netcontroller 2 has a collection of different types of connections, types of comm port connections include RS485, RS232, RS422 and RJ11

Please see attached document for a full list of the Netcontroller 2 pinout configurations Link