Webstation not showing images and formatting is missing

Issue

When Webstation is opened, no images are shown and formatting (styling) is missing

Product Line

TAC Vista

Environment

Webstation

Cause

The Webstation application doesn't have access to or can't parse the stylesheet

Resolution

1: Uninstall Webstation (including hotfixes)

2: Install Webstation by right clicking the installer and selecting "Run as administrator"

3: Run "Webstation Corrections"