NET5500 Series Encoder IP address

Issue

Default IP address for the NET5500 series encoder

Product Line

Pelco Cameras, Pelco Video Management

Environment

NET5500 series.

  • NET5501
  • NET5504
  • NET5508
  • NET5516

Cause

Encoder has been factory defaulted

Resolution

If there is no DHCP server on the network, the NET5500 series encoder will have a default IP address of 192.168.0.20.

Note: The NET5500 series will use one ip address for all the input channel.

 

Also see related article LL#17008 - How to factory default a NET5500 series encoder