What are the available audio/microphone options for Sarix Enhanced (IME Series) IP Cameras?

Issue

What are the available audio/microphone options for Sarix Enhanced (IME Series) IP Camera Systems?

Product Line

Pelco Cameras

Environment

Cause

Pre-sales option selection 

Resolution

Sarix IME Series IP Camera Systems offer audio/microphone support as follows...

  • "Indoor" and "Vandal-resistant" models have a built-in microphone as well as offering the line-in option for use with an external microphone.
     
  • "Environmental" models do not have a built-in microphone, but still offer the line-in option for using external microphone.
    note: see LL#16709 for line-in installation details.
     

The highlighted models offer built-in microphone -