What is the maximum Tilt angle adjustment for the IBP series Environmental Bullet Cameras

Issue

The vertical Angles of view are on teh specification sheet, but what ius the maximum Tilt Angle Adjustment?

Product Line

Pelco Cameras

Environment

  • IBP Series

Cause

  • Sales Support
  • Application Design

Resolution

The maxmimum angle that can be achieved is 85 degree.