What is the Tri-Pod mount size on the IBP Series Environmental Bullet Cameras

Issue

What are the thread size specifications for the Tri Pod mount

Product Line

Pelco Cameras

Environment

  • IBP Series

Cause

  • Sales Support
  • Apllication Design

Resolution

The Mounting hole size for the Tripod mount is:

#10/24 0.041667 \ 1.0583