Changing configuration on Spectra Pro after they have been set up in DSSRV may cause the camera to crash

Issue

Changing configuration on Spectra Pro after they have been set up in DSSRV may cause the camera to crash due to CPU overuse

Product Line

Pelco Cameras, Pelco Video Management

Environment

When using the Spectra Pro with DSSRV

Cause

The DSSRV series send out calls to the cameras with the setting that are done on the VMS. If you channge the settings afterwards in the webUI it causes  CPU problems with the camera.

Resolution

Only change and set up the Spectra Pro in the DSSRV when it is connected to it