The new Spectra HDR Enhanced is not interchangeable with the Spectra HD series


You cannot put a Spectra HD dome into a Spectra HDR Enhanced backbox  or a Spectra HDR into a Spectra HD backbox. Doing so will burn components in either camera or backbox. There are tabs in the HDR Enhanced series to prevent this but it can be forced

Product Line

Pelco Cameras, Pelco Video Management


When using Spectra 1080P or 720P HD series cameras and mixing them with the new Spectra HDR series cameras


The electronics for the power supply and for the domes do not match and are different voltages. If the two are interchanged you will have components burn up


Be aware that the Spectra HD series domes and backboxes are not interchangeable with the Spectra HDR enhanced series