When using Firefox with Quicktime to see video you must refresh the page

Issue

When using Firefox with Quicktime  to view video in the webUI you have to refresh the page after allowing the Quicktime application.  Or you can double click in the video area after applying the QuickTime feature

Product Line

Pelco Cameras, Pelco Video Management

Environment

When using quicktime with firefox to view video

Cause

This is due to the way that Firefox handles the QuickTime video application

Resolution

The work around is to either refresh the page or to double click in the video viewing area after allowing the QuickTime application