What is the FSFP-EGRJ45 used for

Issue

The FSFP-EGRJ45 has no documentation to explain design intent.

What is this product used for.

Product Line

Pelco Transmission & Power

Environment

  •  FSFP-EGRJ45 Transceiver
  • FMCI-PF1POE IP Media Converter
  • FMCI-PG1POE IP Media Converter
  • FMCI-PF1POE IP Media Converter
  • FMCI-PG1POE IP Media Converter
  • FUMS-FFX4TX4 Unmanaged Ethernet Switches
  • FUMS-FTX8 Unmanaged Ethernet Switches
  • FUMS-FFX2TX2 Unmanaged Ethernet Switches
  • FUMS-FTX4 Unmanaged Ethernet Switches

 

 

Cause

Sales Support

Resolution

The FSFP-EGRJ45 is used in an application as a POE injector to pass POE to a powered device.

Existing infrastructure can be utilized when using switches.