Will StruxureWare Building Operation provide any indication of a failure sending a SNMP trap?

Issue

Will StruxureWare Building Operation provide any indication of a failure sending a SNMP trap?

Product Line

SmartStruxure Solution

Environment

AS

ES

SNMP

Cause

Documentation

Resolution

If there is a failure sending an SNMP trap Building Operation will generate a system alarm/event indicating that the trap could not be sent. Note though, that if the trap is sent successfully there is no indication or log entry to indicate so.