When using the Pelco 8 or 16 channel MidSpan injectors the Spectra HD's may take a long time to power up


The Spectra HD series will take as long as an hour to power up with the 8 and 16 channel MidSpan injectors

Product Line

Pelco Cameras, Pelco Video Management, Pelco Transmission & Power


Pelco Mid span injectors, Spectra HD


The Spectra HD series use class 0 PoE and this causes the handshake to  sometimes take a long time to negotiate and make power connection. This is especially true in the 720P series and not as much on the 1080P series


There is no resolution at this time, you may change to a 4 channel or single channel injector. You can try a different brand of injector also