Adding Card Numbers through a Card View Reader

Issue

Adding Card Numbers through a Card View Reader

Product Line

TAC I/NET

Environment

I/NET Site with Access Control

Cause

How does one Add Card Numbers through a Card View Reader

Resolution

In I/NET, if you are using a Card View Reader Plus to read cards into the system there is a simple way to add these cards to Individuals who either have existing cards or no cards.

For example, if a user has several hundred cards that needs to be replaced, instead of deleting the old card and re-issuing a new one, follow these steps:

  1. Click on Access; choose the Tenant and then Individuals. Select the individual that the card is being added to, then read the card.
  2. The number automatically appears in the next line for Hex Numbers.
  3. If there is no number, then it automatically puts it in.
  4. IF the user has Video Badging, all they would need to do is print the badge of the individual that the card is being added for and then read it into the system.