Issue
How to create a write to file notification for an alarm that creates a comma separated value (CSV) file.
Product Line
EcoStruxure Building Operation
Environment
- Struxureware up to v1.7
Cause
Write to file notification to create a CSV file.
Resolution
Under file name, end with the extension .csv.
This will produce a .csv file located in your database folder under the folder Notification.
NOTE
The process changed slightly from v1.8, where Write to file, Email, Client and SNMP Notifications where replaced by "Variable Triggered Notifications" and "Alarm Triggered Notifications" with Write to file, Email, Client and SNMP now set in the "Distribution method" within the Triggered Notification Object
WebHelp is the best source of further information