ES40/ES41 Series Esprit

Issue

Unable to verify if the ES4136-5N and ES4036-5N are IP67 rated?

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • ES44036-5N
  • ES4136-5N
  • ES41P36-5N
  • ES40P36-5N

Cause

User hel Needing to verify IP67 ratings/Certification on ES4036-5N and ES4136-5N.

Resolution

ES4036-5N and ES4136-5N are not IP67 rated. 

To verify Ratings/Certifications on ES4136-5N, ES4036-5N:

Go to www.pelco.com.
Open Spec Sheet for ES40/ES41 Series Positioning System.
Go to page 3 and look under CERTIFICATIONS/RATINGS/PATERNTS.
 

NOTE: ES41P36-5N and ES40P36-5N meets IP67 standards (Esprit with Pressurized IOC)