Issue
Printing the NPR Configuration
Environment
- I/NET Seven
- NPR
Cause
I/NET now has the ability to print the settings for the NPR when it has been configured. This feature should be used anytime an NPR is set up or changed per the user. It is extremely important for use when and if an NPR has to be replaced or loses its settings due to power failure or whatever the issue might be.
Resolution
To use this feature the following steps need to be followed:
- Open I/O Server, NP Routers and modify the active NPR, you can also print the settings of NPRs that are not Online.
- Once the settings come up, click on Print and it will send this information to your default printer or Network Printer of your choice.
- Keep this sheet of paper with all of your other I/NET documentation.