Wire and Configure the IPCT01 IP Camera Tester for Power Over Ethernet (POE) as an Internal Power Source

Issue

The IPCT01 camera installation tool provides Power over Ethernet (POE) support. It connects directly to a camera to provide power using an Internal Power Source.

Product Line

Pelco Cameras

Environment

  • IPCT01 IP Camera Tester all Versions

Cause

  • Installation and Service
  • IPCT01 use as a POE Power Source.

Resolution

Connect a straight ethernet cable from the IP Camera to the LAN / PoE OUT Port on the side of the IPCT01

Make sure the Power Bank switch is in the OFF Position.

From the Main Menu; Tap POE ON  to enable the IPCT01's POE function. The PSE indicator light will be on  which means the Tester is now providing power to the IP Camera.

 

 

The POE ON icon will change to POE OFF when POE is enabled.

 

Tap POE OFF to turn off the POE function.

 

 

Related Topics:

How to Setup Power over Ethernet (POE) on the IPCT01 IP Camera Tester