Why do lens with the same focal lengths have different angles of view when a scene is viewed from the same focal length

Issue

Why do lens with the same focal lengths have different angles of view

Product Line

Pelco Cameras

Environment

All CCTV Lenses

Cause

Different Lens manufacturers uses various glass specifications

Resolution

Different manufacturers design and build specifications, use different glass specifications.