Pressurized Spectra may leak if made before July 14th , 2014

Issue

The pressurized Spectra had an issue with the relief valve leaking. This was due to a specification malfunction  from the vendor that makes the valve

Product Line

Pelco Cameras, Pelco Video Management

Environment

Pressurized Spectra made before July 14th 2014

Cause

The relief valves were faulty and would leak sometimes

Resolution

to replace with new valve made by Generant part number VRV 125B  The old valve was made by Indian peak. The difference is the new one has VRV-125B on it and is chrome plated and the old one is brass