Hasp Key Utility will not activate keyless license Version Error Getting Id. -- Key Id Not Found


Version 2.0a Error getting Key Id appears at bottom of the Hasp Key Utility when an attempt is made to activate the Continuum license using the v2c file. 

Product Line

Andover Continuum


  • Continuum
  • Keyless
  • Soft License
  • Hasp Key Utility
  • Sentinal HASP License Manager


A defect has been identified with Sentinals HASP Runtime executible prior to release 6.56 which can in some cases cause the Hasp key Utility's Key ID number to change each time the host machine is rebooted.     

To determine if this is your issue run the following test:

1. Launch the Hasp Key Utility executible in the Continuum program folder.

2. Select Show Key Information.

3. Note and record the Key ID #.

4. Shut down the Hasp Key Utility and reboot the host machine.

5. Relaunch the Hasp Key Utility and recheck the Key ID#.


If the Key ID has changed following a reboot of the host machine, download the most recent version of the Continuum Software License Upgrade Utility from the Exchange Download Center.