LonMark Resource Files version in SmartStruxure

Issue

SmartStruxure comes preloaded with LonMark's resource files. It is not documented what version of the LonMark Resource Files are build into each version of SmartStruxure.

Product Line

SmartStruxure Solution

Environment

LonWorks

LonMark

Cause

This is missing from the documentation

Resolution

SmartStruxure 1.2: Resource Files version 13.02
SmartStruxure 1.3: Resource Files version 13.02
SmartStruxure 1.4: Resource Files version 13.12
SmartStruxure 1.5: Resource Files version 14.00
SmartStruxure 1.6: Resource Files version 14.00