Component part numbers for the Spectra HD 1080p IP camera


What are the component model numbers for the Spectra HD 1080p?

Product Line

Pelco Cameras


  • S5220
  • S5230
  • D5220
  • D5230


Components required to change a Spectra HD 1080P (D5520/5230) from a in-ceiling to a pendant or vise versa. 


System Model numbers for the Spectra HD are structured for assembly of 3 components that create an all in one package of Back Box (housing), Lower Dome, and Dome Drive (camera). The System model numbers then breakdown to individual component models so that any part may be ordered separate for a field replacement or swap.

Example of a System Model Number: S5220-FW0 consists of B52-F, D5220F, LDHDF-0. If the camera is required to be moved to an outdoor pendant installation, install the B52-PG-E with LDHDPB-0 (smoked) lower dome. The D5220 or D5230 camera is the same model for any housing with matching lower dome. Reference component model number chart below to ensure back box mates with proper lower dome.