Connecting the RS-422/RS-485 Data Wire to a NET5501.

Issue

Don't know how to connect the RS-422/RS485 data wire to the NET5501.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • NET5501
  • Spectra IV Series

Cause

User help

Resolution

Connecting the RS-422/RS-485 data wires to the terminal block:

NOTE: The terminal block has tension clamps instead of screw terminals.
 

  1. Use a small screwdriver to open the clamp for the particular lead (RX-, RX+, TX-, TX+).


     
  2. Insert the Data wire to the corresponding lead (RX+, RX-, TX-, TX+).


     
  3. Let go of the tension clamp once the data wire has been incerted and making good contact.
     

 

PTZ Pin Assignments: