WARNING: Invalid value for ProgramID in the object, ~/LonWorks Local FT-10 Interface/Your_network/Controllername/IO/IO_module_name. The default value has been applied.

Issue

Get Invalid value for ProgramID in the object, "~/LonWorks Local FT-10 Interface/Your_network/Controllername/IO/IO_module_name". The default value has been applied. In the conversion log when upgradeding database

Product Line

SmartStruxure Solution

Environment

AS

Device administrator

Cause

TAC Xenta IO modules of the model 411/421 does not have an application ID populated in the properties. All other IO modules do.

The upgrade sees this as missing information

Resolution

You can ignore this if the module is a TAC Xenta IO 411/412