Fails to connect TAC Vista to SBO Conversion Tool to the PCS server

Issue

Fails to connect TAC Vista to SBO Conversion Tool to the PCS(Project Configuration Server) server. When the PCS server is specified in the TAC Vista to SBO Conversion Tool and trying to do the Convert the following error message is showed:
Server certificate must be trusted permanently from Windows, WorkStation or WebStation. Temporary trust is not supported through the SDK. Exception of type 'SE.WorkStation.IntegrationObjects.Simple.Communication.ErrorException' was thrown.

Product Line

TAC Vista, SmartStruxure Solution

Environment

TAC Vista 5.1.9
StruxureWare Building Operation all versions
TAC Vista to SBO Conversion Tool all versions

Cause

The logon mechanism is not working in the same way for the PCS as it does for the ES

Resolution

The TAC Vista to SBO Conversion Tool is not built and supported for a connection to the PCS only to the ES and AS