A generic error occurred in GDI+


When editing a TGML error A generic error occurred in GDI+ appears

Product Line

TAC Vista, SmartStruxure Solution


  • TAC Vista
  • StruxureWare Building Operation
  • TGML
  • Graphic editor


This issue occurs after you install security update 3045171. You experience a crash when you use Windows GDI+ to create text outline-based path objects on a computer that is running Windows 7 Service Pack 1 (SP1) or an earlier version of Windows.


Download the patch below from Microsoft



It has been noted that this patch do not solves all the issues, if you still have issues with other applications uninstall the security update KB3045171.