Is it possible to bind more than one variable to a Lonworks variable?

Issue

Is it possible to bind more than one variable to a Lonworks variable?

Product Line

SmartStruxure Solution

Environment

SmartStruxure 1.X.X 

LonWorks

Cause

In some instances it is approriate to bind multiple variables to one variable, such as a number of switches bound to one actuator.

Resolution

There are so-called "Fan-In" Bindings that are purpose designed for this.

There are also a number of different binding configurations, that are described in SmartStruxure Building Operation Web Help here.

To be able to bind more variables in Workstation the user must add more rows to the binding field (see screen shot below).