How to reset the Esprit HD to factory default.

Issue

Unable to access Esprit HD web page.

Product Line

Pelco Cameras

Environment

ES5230 Esprit HD Series

Cause

  • IP address is unknown.
  • Firmware corruption.

Resolution

We have two models of Esprit HD both have the ability to be reset from the camera web page.

To reset via camera web page

Login and click on settings, from the System Tab click on Restore all Camera defaults.

 

To reset by physically going to the camera.

The newer Esprit HD will have a reset button located in the housing:

  1. Open the enclosure lid.
  2. Locate the reset shown in the picture below.
  3. Secure the ES5230 by holding the front of the enclosure because the ES5230 will loses power.
  4. Hold the reset button for 20 sec or until power is lost on ES5230.
  5. The ES5230 will take up to 5-10 minutes to re-establish an IP address after reset.