Can the Sarix Professional IP cameras record audio to the internal SD card?

Issue

Can a Sarix Professional IMP IP camera record audio to the internal SD card.

Product Line

Pelco Cameras

Environment

  • Sarix Professional Series
  • IMPS110,IMP219,IMP319,IMP519,IBP,IXP
  • MicroSDHC or MicroSDXC 32GB cards

Cause

The Sarix Professional IP cameras can record video to the internal SD card but audio is not captured.

Resolution

The Sarix Pro series IP cameras support video only capture to the internal SD card, audio is not supported.