ACCDataServices.exe crash

Issue

ACCDataService.exe in ITP.DLL crashes when any function is calling another function. 

Product Line

Andover Continuum

Environment

Continumm 2.0

Cause

When a PE Function is called from within another PE Function.

Resolution

To resolve this issue the following steps need to be followed:

  1. Do not call up a PE function from within another PE function
  2. Copy the script code function from the second function and put it directly into fthe first function.