Not all traffic on a segment is captured when using the LPA through an Automation Server

Issue

When using the LPA through an Automation Server (AS) as described in article #16285, only traffic to and from the AS is captured.

Product Line

SmartStruxure Solution

Environment

LPA

Automation Server

Cause

Due to a hardware limitation in the AS, it's not possible to capture all traffic on the segment

Resolution

Connect the LPA to the segment using a NIC-USB100 or similar