RJ10 Pin Out for Xenta OP

Issue

RJ10 Pin Out for Xenta OP

Product Line

TAC Vista

Environment

Xenta OP

Cause

The Xenta OP has two connection methods, the 4 pin terminal blocks and an RJ10 port. Some users have the need to make custom RJ10 cables.

Resolution

The pin order for the RJ10 port is the exact same as the order on the terminal block right next to it. From right to left they are:

  1. C1 (comms 1)
  2. C2 (comms 2)
  3. G+ (power)
  4. G0 (ground)