How Do I Enable DHCP on the IPCT01


Configure the IPCT01 for DHCP address assignment.

Product Line

Pelco Cameras


IPCT01 all versions


Network Setup


To power on the IPCT01, please set the Power Slide Switch on the side to “ON” position, and press and hold the Start Key for 3 seconds.

Navigate menus: click on Setup => Setup IP => Setup IP Connection

  1. Click on the DHCP button
  2. The Tester Address field greys out. 
  3. Click on SET to send out a DHCP request.