Windows installer fails to install an application

Issue

Windows installer fails to install an application

Product Line

TAC I/NET, TAC Vista, Andover Continuum, Satchwell MicroNet, Satchwell Sigma, TAC I/A Series, SmartStruxure Solution, Other, Pelco Matrix, SmartStruxure Lite

Environment

  • Microsoft Windows Server 2003
  • Microsoft Windows Server 2003 R2
  • Microsoft Windows XP
  • Windows 7
  • Windows Server 2008
  • Windows Server 2008 R2
  • Windows Vista
  • Windows 8
  • Windows 8.1
  • Windows Server 2012 editions
  • Windows Server 2012 R2

Cause

Errors with the Windows Operating system are preventing the installation from completing.

Resolution

Run the file at the link below on the affected PC:

 

https://support.microsoft.com/en-us/mats/program_install_and_uninstall